I wanted to post the details of my project to change the MCUXpresso example code for a generic HID device from full to high speed and increasing the packet size. I tried to do a blog post but all the "places" are grayed out. What is the commonly accepted place to put this kind of post?
The dev baord is the LPCXpresso54608 / OM13092. The example code was from the MCUXpresso SDK for this board, but it is nearly identical to the generic HID code for other Kinetis MCUs as well. I tested the packet size changes on the K22 tower board TWR-K22F120M.
已解决! 转到解答。
Hi Nick,
I got answer from our community manager.
"
Users don't have permissions to create blogs or documentation, just the admin and moderator can do it.
The user option is to create a discussion, next if the Support team or an admin/moderator consider the info valuable, this can be converted to a document.
"
If you would like to convert the discussion to document, you can send me internal message. I can help to check.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Nick,
In addition of Erich, Can you please also share screenshot of " all the "places" are grayed out"? I may try if we can find out the problem inside support team.
Best Regards,
Jennie Zhang
Thanks for your quick replies. I would have responded sooner, but has a major delay due to ransomware.
Here is a screen pic of the grayed out options when trying to pick a blog place (all options in the scroll list are gray/non-selectable):
Hi Nick,
I got answer from our community manager.
"
Users don't have permissions to create blogs or documentation, just the admin and moderator can do it.
The user option is to create a discussion, next if the Support team or an admin/moderator consider the info valuable, this can be converted to a document.
"
If you would like to convert the discussion to document, you can send me internal message. I can help to check.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks for the info. I had a feeling that was the case. Not sure why they would make "blog" as an option considering what you have shared though.
I'm fine with leaving it as a discussion. It's searchable so if others are interested, they should be able to find it.