Unable to run SDK code samples on FRDM-K32L2B3 board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to run SDK code samples on FRDM-K32L2B3 board

2,477 Views
ClaudeHenry
Contributor I

I'm testing the FRDM-K32L2B3 evaluation board using MCUXpresso SDK and IDE as described on the "Getting Started" page but the MCU is unable to run the generated SDK sample code.

I did exactly the following:

  • Open URL https://www.nxp.com/design/development-boards/freedom-development-boards/mcu-boards/nxp-freedom-deve...
  • Click on "GET STARTED"
  • Click on "Jump To => 2. Get Software"
  • Click on "GET MCUXPRESSO SDK" (Download SDK_2_6_0_FRDM-K32L2B.zip)
  • Click on "GET MCUXPRESSO IDE" (Download MCUXpressoIDE_11.4.1_6260.exe)
  • Click on "Jump To => 3. Build Run"
  • Click on "USE MCUXPRESSO IDE" (Open "Running a demo using MCUXpresso IDE" document)
  • Install "MCUXpressoIDE_11.4.1_6260.exe" and open the IDE
  • Drag and Drop the file "SDK_2_6_0_FRDM-K32L2B.zip" into the "Installed SDKs" view
  • Click on "Import examples from SDK" in the "Project Explorer" view (Show the selected "frdmk32l2b" SDK)
  • Click on "Next"
  • Select the example "demo_apps / led_blinky"
  • Click on "Finish"
  • Click on the "frdmk32l2b_led_blinky" project
  • Click on "Build"
  • Click on "Debug"
    Panel "Probes discovered" pop up and show the "CMSIS-DAP" available probe.
  • Click on "OK"

Debug result in this screenshot: 

Screenshot 2021-10-12 083517.png

I tried also the "hello_word" code sample with the same result. 

 

Thanks' for your help.

Claude

 

0 Kudos
16 Replies

2,375 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello @ClaudeHenry ,

 

Please find a guide provided by us that could help you out. Please let me know anything else.

Production Flash Programming Best Practices for Kinetis K- and L-series MCUs 

0 Kudos

2,358 Views
ClaudeHenry
Contributor I

Hi,

I didn't find anything that can help me to fix the issue actually.

I did the flash mass erase with the MCUXpresso IDE but this doesn't fix the issue.

I would like to use the "blhost" tool to try to flash the MCU but I didn't find a way to reset the MCU in BOOTROM mode.

Normally I should be able to do that by pressing the button 2 (connected to the NMI) during power up or MCU reset.

Also, is there a way to program the flash FTFA option bits with the MCUXpresso IDE ?

 

Regards,

 

Claude

 

0 Kudos

2,342 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello @ClaudeHenry ,

In the previous attached guide I will recommend to follow the SWD mas erase procedure in your particular case.

0 Kudos

2,323 Views
ClaudeHenry
Contributor I

Hello,

I would like to do the SWD flash erase, but I don't know how to do this on my evaluation board FRDM-K32L2B3.

Do I need a special hardware probe plugged on the J11 connector with dedicated software tool, or can I do that via the on board OpenSDA ?

 

Regards

Claude

 

0 Kudos

2,317 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello @ClaudeHenry ,

You can refer to the following post for the SWD.

How to trigger mass erase on somehow locked K32L2A 

Also as you have mcuxpresso you can do a mass erase by using the GUI Flash tool available within the IDE. For instructions on how to use it, please check Chapter 14 of the MCUXpresso IDE User Guide. 

0 Kudos

2,308 Views
ClaudeHenry
Contributor I

Hello,

I already tried to do the mass erase with MCUXpresso IDE but this didn't solve the issue.

Also I can read the flash, so it doesn't seem to be read protected.

 

Regards,

 

Claude

 

0 Kudos

2,284 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello @ClaudeHenry ,

Can you please try with updating your OpenSDA this could also be causing your issue.

OpenSDA 

The SWD it can be performed through openSDA.

0 Kudos

2,402 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello @ClaudeHenry 

 

Ok, you can follow the next guide that can help you unlock and erase your MCU.

On the section Unlocking and Erasing with J-Link Commander.

https://mcuoneclipse.com/2014/10/05/unlocking-and-erasing-flash-with-segger-j-link/

0 Kudos

2,384 Views
ClaudeHenry
Contributor I

Hello,

 

It would be a good idea but we don't  have the Segger J-Link probe.

We only have the on board OpenSDA.

Is it possible to do the same thing using the NXP "blhost.exe" application and in this case, how to do it ?

 

Thanks' for your help

 

Claude

 

0 Kudos

2,464 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello @ClaudeHenry ,

I recommend to use the SDK latest version for the K32L2B that can be found on the following link. It is version 2.10.0

 

FRDM-K32L2B

SDK FRDM-K32L2B 

0 Kudos

2,461 Views
ClaudeHenry
Contributor I

Thanks', but I tried the latest v2.10.0 with the same result.

 

Claude

 

0 Kudos

2,456 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello @ClaudeHenry,

 

I also have a K32L2B3 evaluation board and I can flash a demo with no problems so we can discard a SDK problem.

In this case there are a couple questions:

  1. When you connect your board to your PC before doing anything else you receive a message from your PC that shows that the device has been detected? Also can you please re-check your device manager.
  2. When you connect your board, do you see a green led blink? It is located over the SDA port.
  3. Are you connecting your board in the J13 Power/OpenSDA otherwise if you are connected to the J10 K32L2B3 USB it won't works as it should.
  4. Is this the first time you use this EVAL board?
0 Kudos

2,451 Views
ClaudeHenry
Contributor I
  1. The device is detected and we can see the COM3 serial port and the CMSIS-DAP in the device manager.
  2. I can see the green LED blinking when I connect the board.
  3. I am connecting the board in the J13 Power/OpenSDA.
  4. It is the first time I use this eval board.

Regards,

Claude

 

0 Kudos

2,435 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello @ClaudeHenry ,

 

Thanks for answering my questions, can you please create a new workspace and place the latest version of the SDK and let me know if this works.

It does not seem to be something wrong with your board.

0 Kudos

2,414 Views
ClaudeHenry
Contributor I

Hi,

 

I tried a new evaluation board out of the box and all is working fine on this one.

The bad board was flashed first with an application developed on the Zephyr platform.

Is there a specific procedure to reset this board to factory settings for example ?

 

Regards,

 

Claude

 

0 Kudos

2,426 Views
ClaudeHenry
Contributor I

Hello,

 

The board was working fine with until I try to load this new software.

I suppressed all SDKs and reinstall the last one 2.10.0.

The result is the same.

Capture.PNG

0 Kudos