Hello,
Importing lpc11u68 board library, lpc11u68 chip library & USBD library projects using the TN00036.zip archive does not place source files within its associated project for lpcxpresso board. I need clarification on how to complete successful build of each project.
• MCUXpresso IDE v11.2.1 [Build 4149] [2020-10-07].
• TN00036.zip.
• Technical note, TN00036 USBD Library for LPC1100 series MCUs. 1.0 — 13 March 2018 (pdf document).
• OM13058: LPCXpresso Board for LPC11U68, v2 Rev B.
I am attempting to import the latest board, chip, & USBD libraries from the TN00036.zip (into a new workspace), as detailed in the accompanied TN00036 technical note pdf.
Importing lib_chip_11u6x and lib_board_nxp_lpcxpresso_11u68 projects using the file system projects archive places the source and include files outside the project filesystem, as specified in both the \prj_xpresso11u68\lpcxpresso\lpc_chip_11u6x\.project & \prj_xpresso11u68\lpcxpresso\lpc_board_nxp_lpcxpresso_11u68\.project files' <linkedResources> XML tags.
The subsequent build of these projects fail. I can work-around this problem by deleting the Linked Resources properties of each project, creating src & inc project source folders and importing the appropriate files into the folders.
The technical note states that the USBD library can be found under:
\usbd_lib_lpc11u6x\prj_lpc_usbd_lib. The import file system project archive: lpc_usbd_lib ( usbd_lib_lpc11u6x\prj_lpc_usbd_lib\mcuxpresso) does not create src or inc folders.
I assume that I need to add these source folders and imports files from \usbd_lib_lpc11u6x\LPC_USBD_Lib\mw_usbd, \usbd_lib_lpc11u6x\LPC_USBD_Lib\mw_common & \usbd_lib_lpc11u6x\LPC_USBD_Lib\hw_usbd_ip3511 folders.
已解决! 转到解答。
I hadn't needed to use linked resources before. The penny dropped after reading to following stack overflow question:
I needed to edit the project's Properties > Linked resources > Linked resources tab. and ensure that the link location points to the file location of the named resources. For example:
Resource name: board.c
Location: WORKSPACE_LOC\..\TN00036\usbd_lib_lpc11u6x\brd_xpresso11u68\src\board.c
Thanks for testing my issue and your prompt response.
However, your reply doesn't detail how you resolved the issue. Could you please provide a full explanation of what you did to successfully build all three chip, board, and USBD libraries.
Best regards.
I hadn't needed to use linked resources before. The penny dropped after reading to following stack overflow question:
I needed to edit the project's Properties > Linked resources > Linked resources tab. and ensure that the link location points to the file location of the named resources. For example:
Resource name: board.c
Location: WORKSPACE_LOC\..\TN00036\usbd_lib_lpc11u6x\brd_xpresso11u68\src\board.c