'USB MIDI device' support for MIMXRT1024 MCU?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

'USB MIDI device' support for MIMXRT1024 MCU?

682 Views
simmania
Contributor III

Hi,
I'm investigating if I can use the MIMRT1024 for my new project.
I want to build a MIDI keyboard that connects using USB.
I searched this forum, but it is not clear to me if support for a 'USB MIDI device' is available for the MIMXRT1024 device.
So is there?
If so, where can I find that?
If not, is there some third party support?

0 Kudos
Reply
4 Replies

617 Views
simmania
Contributor III

Thanks @ZhangJennie for the link!
I also found the Teensy board (Arduino like) that has a MIMXRT1062 chip. It comes with an USB MIDI example. I tested it and it worked.
Can I use that some how in combination with the AN above to create a USB MIDI for MCUExpress? Or does MCUExpress things completely different and it it difficult to merge with some other USB MIDI implementation?

0 Kudos
Reply

652 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hello simmania 

Unfortunately we don't have  'USB MIDI device'. All available USB demos are enclosed in SDK package:

https://mcuxpresso.nxp.com/en/select

Hope this will help you,

Jun Zhang

0 Kudos
Reply

647 Views
simmania
Contributor III

Is there any USB firmware that we can adapt? E.g. a USB Audio Class Device?

I tried your link, but I can not select a MIMXRT1024 MCU. So I do not understand how to use that.

Any help to find out if and how we can create this USB MIDI product using a MIMXRT1024 would be very welcome!

0 Kudos
Reply

638 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi simmania 

In SDK you may find usb_device_audio_generator and usb_device_audio_speaker, and we also provide an AN for that topic, you may refer to
https://www.nxp.com.cn/docs/en/application-note/AN4665.pdf

for more details.

Hope this will help you.

Jun Zhang

0 Kudos
Reply