I am using the NXP LPCXpresso54628. I have a USB HID device that is implemented in RTOS. I want to create a function that is executed when the usb is disconnected from a computer.
I have looked in the hid_generic.c and placed breakpoints in the functions:
static usb_status_t USB_DeviceHidGenericCallback(class_handle_t handle, uint32_t event, void *param)
and
static usb_status_t USB_DeviceCallback(usb_device_handle handle, uint32_t event, void *param)
but no callback is generated when the device is disconnected.
How can I implement this callback ? What are your suggestions ?
Thanks in advance,
Jim
已解决! 转到解答。
Hi Jim,
To do this you need to enable detach feature by setting the following define in usb_device_config.h file.
#define USB_DEVICE_CONFIG_DETACH_ENABLE (1U)
This will enable notification to the device callback through USB_DeviceAttachNotification and USB_DeviceDetachNotification functions.
#if USB_DEVICE_CONFIG_DETACH_ENABLE
case kUSB_DeviceNotifyDetach:
status = USB_DeviceDetachNotification(handle, message);
break;
case kUSB_DeviceNotifyAttach:
status = USB_DeviceAttachNotification(handle, message);
break;
#endif
Now you can implement what you like to do in USB_DeviceCallback when this events occurred. I just print message a in console.
usb_status_t USB_DeviceCallback(usb_device_handle handle, uint32_t event, void *param)
{
usb_status_t error = kStatus_USB_Error;
switch (event)
{
case kUSB_DeviceEventAttach:
usb_echo("USB device attached\r\n");
break;
case kUSB_DeviceEventDetach:
usb_echo("USB device detached\r\n");
break;
Hope it helps!
Best regards,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored.
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------
I have a similar problem same problem on IMXRT1052;
I did #define USB_DEVICE_CONFIG_DETACH_ENABLE 1U
but no event is triggered in the low level isr in the first place when the cable is disconnected;
a breakpoint on USB_OTG1_IRQHandler and USB_OTG2_IRQHandler does nothing when the cable is disconnected,
but attach and other events work correctly
Hi Jim,
To do this you need to enable detach feature by setting the following define in usb_device_config.h file.
#define USB_DEVICE_CONFIG_DETACH_ENABLE (1U)
This will enable notification to the device callback through USB_DeviceAttachNotification and USB_DeviceDetachNotification functions.
#if USB_DEVICE_CONFIG_DETACH_ENABLE
case kUSB_DeviceNotifyDetach:
status = USB_DeviceDetachNotification(handle, message);
break;
case kUSB_DeviceNotifyAttach:
status = USB_DeviceAttachNotification(handle, message);
break;
#endif
Now you can implement what you like to do in USB_DeviceCallback when this events occurred. I just print message a in console.
usb_status_t USB_DeviceCallback(usb_device_handle handle, uint32_t event, void *param)
{
usb_status_t error = kStatus_USB_Error;
switch (event)
{
case kUSB_DeviceEventAttach:
usb_echo("USB device attached\r\n");
break;
case kUSB_DeviceEventDetach:
usb_echo("USB device detached\r\n");
break;
Hope it helps!
Best regards,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored.
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
------------------------------------------------------------------------------