I have an application for TFT128x160, in this application I have the CS / RES / DI / WR / RD and D0 ~ D7 ports.
I am using MK22FX512Axxx12, I need to write 8 bits on ports D0 ~ D7, what is the best way to declare and write on D0 ~ D7 (8 bits)
*** Attached (PDF) is the full summary
Solved! Go to Solution.
Hi Marcel,
To write to D0 to D7 please make sure you:
gpio_pin_config_t config = {
kGPIO_DigitalOutput,
0,
};
GPIO_PinInit(GPIOD, pin, &config);
To write data your approach using PDOR is correct.
Best regards,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Marcel,
To write to D0 to D7 please make sure you:
gpio_pin_config_t config = {
kGPIO_DigitalOutput,
0,
};
GPIO_PinInit(GPIOD, pin, &config);
To write data your approach using PDOR is correct.
Best regards,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------