Hi together.
I have big problems with starting and getting a connection between my new OM13078 Board (LPC1115) and MuxPresso.
I can`t see the board in the software and I don`t know what`s to do now...?
When I connect the board with my USB Port on the PC the ringtone is played but I can not find them in the device manager...
Did I have to install some special drivers or something?
Thank`s for any help and
Best regards
Michi :smileyhappy:
Hi Alice.
Ok I figured it out :smileyhappy:
I was on the wrong page in the programm (in the periphals site...)
Everything is working right i think!
But is there a way to build and load it in to the uC in one step?
Now i klick on build and then click on programm and then i need to select the programmer and the file (there are always written there but i have to klick ok again) and then programm.
It is a little bit stupid ... :smileysilly:
Best regards
Michi
Hi Alice.
I use Win 10. I have tried to install the driver. But there is allways the follow message:
"The driver could not be installed. No mbed Microcontrollers were found."
I see in the mouse and keyboard settings the device: NXP CMSIS-DAP
But is that right there?
I already can not see it in the MCUXpresso.
Thank`s for any help!!
Michi
Hello Sutter,
Sorry I made some mistake.
I test this board on my side (Win10), just click "Debug" button under Quickstart Panel on MCUXpresso IDE:
How about on your side?
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello Sutter Sutter,
What about the system of your PC?
If windows, please try to download and install mbed Windows serial port driver:
Windows serial configuration - Handbook | Mbed
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------