MCUxpresso can't find TWRKV31F120M card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUxpresso can't find TWRKV31F120M card

1,195 Views
GaryOlmstead
Senior Contributor I

Hi --

I have an MV31F120M tower board with the elevator boards set up.  All Jumpers are verified to be in their default positions, and a USB connector is plugged into the board, not the Tower's USB port.  I used the Quick Start Guide to load MSD-DEBUG-TWR-KV31F120M_Pemicro.SDA.  I cycled the USB plug as instructed.  Windows 10 detected a new drive, but not the serial port or the OpenSDA driver.  I have some contact with the board, as every time I plug it in, a window pops up with the BOOTLOADER drive selected. 

Then I went to MCUxpresso, where I have the SDK for this processor and board.  I selected the Hello World demo program.  Somewhere in the process I found a form with a box that specified OpenSDA, so I selected that (although I can't find it now).

Despite all that, MCUxpresso can't find the probe.

On the board, the green LED is flashing.

How can I get MCUxpresso to see the OpenSDA port?  Or, how can I connect the Multilink Universal FX JTAG cable to the board?

Gary Olmstead

0 Kudos
Reply
2 Replies

1,131 Views
zaharr_
Contributor II

Hi Gary, 

Can you please open SDA_INF.HTM file in your bootloader mass storage device and copy and paste the versions of Bootloader and the application that is programmed into the OpenSDA processor. 

It sounds like you might need to update a Bootloader to the latest version that is compatible with Windows 10. 

I am attaching the latest version of TWR-KV31F12 openSDA firmware as well as the latest version of Bootloader to this forum thread. 

In terms of using the Multilink FX under MCUXpresso, you can plugin your multilink into a debug header on the board, set the power jumper inside of the USB Multilink FX to provide power to device, and then start a debug session.

Below are the links to two very useful forum posts:

1. On updating the Bootloader and firmware on OpenSDA board:

https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-fre...

2. Using PEmicro debug interfaces under MCUXpresso:

http://www.pemicro.com/blog/index.cfm?post_id=130

Best Regards,
Zahar

PEmicro. 

0 Kudos
Reply

1,137 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Gary:

Do you use the latest MCUXpresso IDE 11.2.0?

If this issue still exists, I would suggest you update the firmware application, Segger Jlink V1 or P&E Micro v118.

Please refer to below link for more information

OpenSDA Serial and Debug Adapter | NXP 

pastedImage_3.png

https://www.nxp.com/design/microcontrollers-developer-resources/ides-for-kinetis-mcus/opensda-serial...

Regards

Daniel

0 Kudos
Reply