MCUXpresso did not find the toolchain project in the specified directory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso did not find the toolchain project in the specified directory

ソリューションへジャンプ
3,190件の閲覧回数
2541162274
Contributor II
This is my first time using MCUXpresso Config Tools. I downloaded the SDK file according to the video in the Quick Start, but the following error occurred. I don’t know why, I hope someone can help me

pastedImage_1.png

pastedImage_2.png

ラベル(1)
1 解決策
2,709件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello,

what IDE are you using? The first options is meant for (already) created project in the IAR, Keil, etc. You should not point it to the downloaded SDK. The standalone Config Tools does not allow open configuration from MCUXpresso IDE.

If you use the MCUXpresso IDE, it can create a project for you and it also contains the Config Tools integrated. 

From the screenshot it seems that you are using the tools version 4.0. Since May there is newer version 4.1 which I recommend to use.

Regards,

Libor 

元の投稿で解決策を見る

5 返答(返信)
2,709件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Jason.

In addition of Libor, if you want to create a new configuration with standalone Config Tool,

pastedImage_1.png

For detail, see attached video.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,709件の閲覧回数
2541162274
Contributor II

Thank you very much .I have found the problem and known MCUXpresso IDE have config and many other tools intergreted.It's very kind of you to provide the attached video.

0 件の賞賛
返信
2,709件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

Jennie Zhang

0 件の賞賛
返信
2,710件の閲覧回数
liborukropec
NXP Employee
NXP Employee

Hello,

what IDE are you using? The first options is meant for (already) created project in the IAR, Keil, etc. You should not point it to the downloaded SDK. The standalone Config Tools does not allow open configuration from MCUXpresso IDE.

If you use the MCUXpresso IDE, it can create a project for you and it also contains the Config Tools integrated. 

From the screenshot it seems that you are using the tools version 4.0. Since May there is newer version 4.1 which I recommend to use.

Regards,

Libor 

2,709件の閲覧回数
2541162274
Contributor II

Thank you very much .I have found the problem and known MCUXpresso IDE have config and many other tools intergreted.

0 件の賞賛
返信