MCUXpresso and JLINK

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso and JLINK

1,039件の閲覧回数
giannigrondona
Contributor III

Hi

I use LPC54608 as microprocessor  and MCUXpresso as IDE.. I use JLINK tool to download code into my target. The problem I can't program external flash memory, The internal memory is corrected programmed but none location of external memory has been programmed. If I use JLINK with a line command tool from SEGGER I am able to program all memories of my board so I suppose there is no problem from JLINK.

I don't know the reason of this problem, It also happen with the last version of MCUXpresso IDE

Best Regards

Giovanni Grondona.

タグ(1)
0 件の賞賛
返信
1 返信

734件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Giovanni,

Are you using the on-bard debugger with the J-link firmware or an external j-link programmer?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信