kds to mcuxpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kds to mcuxpresso

773 Views
ALP1
Contributor I

is possible to migrate a KDS project to Mcuxpresso?

0 Kudos
1 Reply

593 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello

There is a tutorial aobut import project from KDS to MCUXpresso IDE:

MCUXpresso IDE: Importing Kinetis Design Studio Projects | MCU on Eclipse 

While I think the easy way it create a new project on MCUXpresso ,

and then copy in the custom source code and other modifications. Minimal code re-write should be required since the drivers are the same. They are also both Eclipse/GCC based IDEs so predefines should be straight forward to port over. 

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos