MCUXpreso cannot connect to MIMXRT1060-EVKB board via J-Link or CMSIS-DAP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpreso cannot connect to MIMXRT1060-EVKB board via J-Link or CMSIS-DAP

ソリューションへジャンプ
478件の閲覧回数
Ryszard
Contributor I

This is my first attempt with MIMXRT1060-EVKB. I tried to run the example "helo word" and I could not upload the program. J-Link and CMSIS-DAP do not connect to MIMXRT1060-EVKB either. I do not know what to do next. Please help me what I can do.

0 件の賞賛
返信
1 解決策
443件の閲覧回数
Ryszard
Contributor I

Thanks for the quick response. A little effort and I solved the problem. Everything was in the article "Using J-Link with MIMXRT1060-EVKB or MIMXRT1040-EVK"
https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-J-Link-with-MIMXRT1060-EVKB-or-MIMXRT1040-...

J-Link works ok.

Ryszard

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
450件の閲覧回数
HangZhang
NXP Employee
NXP Employee

Hi @Ryszard 

Are you using the MCUXpresso IDE?

If you use it.

You can download the SDK_2_15_100_MIMXRT1060-EVKB SDK on the NXP official site.

Select Board | MCUXpresso SDK Builder (nxp.com)

And import the downloaded SDK in MCUXpresso.

HangZhang_0-1720433701272.png

And import the example in SDK.

HangZhang_1-1720433730423.png

And click the debug to run the hello world.

Hope this will help you.

BR

Hang

0 件の賞賛
返信
444件の閲覧回数
Ryszard
Contributor I

Thanks for the quick response. A little effort and I solved the problem. Everything was in the article "Using J-Link with MIMXRT1060-EVKB or MIMXRT1040-EVK"
https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/Using-J-Link-with-MIMXRT1060-EVKB-or-MIMXRT1040-...

J-Link works ok.

Ryszard

0 件の賞賛
返信