MCU-Link Pro Debug Probe fails on just 1 laptop.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCU-Link Pro Debug Probe fails on just 1 laptop.

1,820 Views
rjleiser
Contributor II

I have 2 MCU-Link Pro Debug Probes.

Using the MCUXpresso IDE v11.8.0 [Build 1165] [2023-07-26].

The probes are all on version 3.

C:\nxp\LinkServer_1.2.45>LinkServer probes
# Description Serial
--- ------------------------------------ -------------
1 MCU-LINK Pro (r0CF) CMSIS-DAP V3.108 TNXNW2C5H4MVO

1 works OK, then other probe fails to open.

I have tried on a different laptop, both probes work.

Within the console:

- Good Probe Connected:


#PROBENUM
1

# ProbeList
Index = 1
Manufacturer = NXP Semiconductors
Description = MCU-LINK Pro (r0CF) CMSIS-DAP V3.108
Serial Number = 2FLE0LKCN3W3I
VID:PID = 1FC9:0143
Path = 0002:0028:00

# ProbeStatus
Index = 1
Manufacturer = NXP Semiconductors
Description = MCU-LINK Pro (r0CF) CMSIS-DAP V3.108
Serial Number = 2FLE0LKCN3W3I
VID:PID = 1FC9:0143
Path = 0002:0028:00

IsOpen = FALSE
WireInitialized = FALSE
WireProtocol = JTAG
CoresConfigured = FALSE
PacketSize = 512
Reference Count = 0
HasSWV = FALSE
HasETM = FALSE
HasJTAG = TRUE
HasSWD = TRUE
HasBOOTCTRL = TRUE
Probe Type = CMSIS-DAP

Probe Reference Count = 0

# ProbeOpenByIndex 1
Probe Handle 1 Open

- Bad Probe Connected:

#PROBENUM
1

# ProbeList
Index = 1
Manufacturer = NXP Semiconductors
Description = MCU-LINK Pro (r0CF) CMSIS-DAP V3.108
Serial Number = TNXNW2C5H4MVO
VID:PID = 1FC9:0143
Path = 0002:0027:00

# ProbeStatus
Index = 1
Manufacturer = NXP Semiconductors
Description = MCU-LINK Pro (r0CF) CMSIS-DAP V3.108
Serial Number = TNXNW2C5H4MVO
VID:PID = 1FC9:0143
Path = 0002:0027:00

IsOpen = FALSE
WireInitialized = FALSE
WireProtocol = JTAG
CoresConfigured = FALSE
PacketSize = 512
Reference Count = 0
HasSWV = FALSE
HasETM = FALSE
HasJTAG = TRUE
HasSWD = TRUE
HasBOOTCTRL = TRUE
Probe Type = CMSIS-DAP

Probe Reference Count = 0

# ProbeOpenByIndex 1
Error: Probe not open

Apart from the 1 probe now working, the only difference I can see is this:

Path = 0002:0027:00

Path = 0002:0028:00

I have tried uninstalling and reinstalling drivers. But nothing changes.

MCU-LINK_INSTALLER_3.108.exe

0 Kudos
14 Replies

1,699 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I have more questions, what MCU are you using as a target? what is the OS do you have? this is the first time that this error has happened. I mean, could you be available to flash the target in the past? Do both devices have the same position jumpers? 

Best regards,
Pavel

0 Kudos

1,684 Views
rjleiser
Contributor II

OS: Windows 10 Enterprise

OS Version: 10.0.19045 Build 19045

The jumpers are identical on the probes.

LPC54606

 

 

0 Kudos

1,679 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, could you try this version, please? Let me know if the behavior still persists.

Pavel_Hernandez_0-1696976025242.png

MCU-Link Pro Debug Probe | NXP Semiconductors

Best regards,
Pavel

0 Kudos

1,596 Views
rjleiser
Contributor II

MCU-Link installer for Windows (WinUSB, MCUXpresso 11.7 or later) FEATURED

EXERev 3.108Jan 16, 2023 16:00:002.1 MBMCU-LINK_INSTALLER_3.108_WIN
 
0 Kudos

1,657 Views
rjleiser
Contributor II

 

I am running IDE version 11.8.

I do not believe the version 2 of the probe is compatible. It needs to be version 3.

 

0 Kudos

1,586 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, I suggest doing the test with version 2, if this still does not work, I'm afraid this is an isolated problem that only happens on your laptop because the MCU link works on the other PC.

Best regards,
Pavel

0 Kudos

1,164 Views
rjleiser
Contributor II

I bought a 3rd probe.

I updated it to version to version 3. And it works. So that suggests there is some esoteric issue with the probe and not necessarily my laptop.

 

All 3 probes have identical markings:

700-5003 rev A

SCH-5053 rev A1

The serial numbers are different:

EA-W01264-0091 (doesn't work)

EA-W01264-0219 (works)

EA-W01264-0398 (works)

0 Kudos

1,152 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, sorry for the inconvenience this may cause, I reviewed the information, and in some cases is because the driver of the USB is not recognized by the PC. I reviewed your setup seems good, but I found this is the only difference. I recommend doing the test with the last version 2.xx to get more details about this behavior.

Pavel_Hernandez_1-1699998160319.png

In another way, as a test I recommend checking the J-Link driver maybe this could help you with this curious issue.

Pavel_Hernandez_2-1699998721108.png

Best regards,
Pavel

0 Kudos

1,711 Views
rjleiser
Contributor II

What does this mean?

Path = 0002:0027:00

Path = 0002:0028:00

0 Kudos

1,804 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, my name is Pavel, and I will be supporting your case, I recommend reviewing this page, you could try to change the flavor of the firmware. 

I do not have the latest version on my PC, but this is the root, only need to put the DFU and run the script.

Pavel_Hernandez_0-1696368710560.png

Best regards,
Pavel

0 Kudos

1,770 Views
rjleiser
Contributor II

It doesn't change anything.

 

Please keep in mind that the probe works on a different laptop. both probes work there.

On my laptop just 1 probe works, the other probe fails.

0 Kudos

1,752 Views
Pavel_Hernandez
NXP TechSupport
NXP TechSupport

Hello, this is a curious case, in that way, I suggest updating the driver 1 by 1 the driver in the device manager, maybe there is a conflict with that.

Image as an example.

Pavel_Hernandez_0-1696543597344.png

Best regards,
Pavel

0 Kudos

1,713 Views
rjleiser
Contributor II

rjleiser_0-1696840057101.png

I have tried this.

I have tried deleting the drivers program, and falling back to the default microsoft usb drivers. But it is still the same. 

If I have 1 probe that works, doesn't that suggest that the drivers are OK?

0 Kudos

1,815 Views
rjleiser
Contributor II

00000.000 MCUXpresso IDE RedlinkMulti Driver v11.8 (Jul 12 2023 16:09:15 - crt_emu_cm_redlink build 2)

( 0) Reading remote configuration

Wc(03). No cache support.

00002.264 Found chip XML file in C:/Users/leiser-1/Documents/MCUXpressoIDE_11.8.0_1165/workspace/OPGMkX_54606_1/Debug\LPC54606J512.xml

( 5) Remote configuration complete

00002.265 emu ConnectToServer

00002.266 Reconnected to existing LinkServer process.

00002.266 emu ConnectProbeCore 1 0 0 0x8000

00002.280 emu ProbeCore failed 0xA2

00002.280 Connecting to probe 1 core 0 (using server started externally) reports:

'Ee(42). Could not connect to core.'

00002.280 Retrying...

00002.789 emu ConnectProbeCore 1 0 0 0x8000

00002.803 emu ProbeCore failed 0xA2

00003.317 emu ConnectProbeCore 1 0 0 0x8000

00003.336 emu ProbeCore failed 0xA2

00003.844 emu ConnectToServer

00003.845 Reconnected to existing LinkServer process.

00003.845 emu ConnectProbeCore 1 0 0 0x8000

00003.863 emu ProbeCore failed 0xA2

00004.369 Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.

Failed on connect: Ee(42). Could not connect to core.

No connection to chip's debug port

(100) Target Connection Failed

0 Kudos