I'm trying to migrate my old project implemented in KDS3.2 (with PE) to MCUXpresso.
Using Bits1_PutVal(Bits1_Ptr…… instructions I have delayed "Low" sequence between four Outputs.
As a test case I prepared small direct register access program which is working well
While(1)
{
GPIOD->PDOR = 0x1;
DELAY;
GPIOD->PDOR = 0x2;
DELAY;
GPIOD->PDOR = 0x4;
DELAY;
GPIOD->PDOR = 0x8;
DELAY;
}
When I tried to implement the above using API the only solution that I found is adding additional GPIO_ClearPinsOutput() which clears all outputs
While(1)
{
GPIO_SetPinsOutput(GPIOD, 0x1);
DELAY;
GPIO_ClearPinsOutput(GPIOD, 0x1);
GPIO_SetPinsOutput(GPIOD, 0x2);
DELAY;
GPIO_ClearPinsOutput(GPIOD, 0x2);
GPIO_SetPinsOutput(GPIOD, 0x4);
DELAY;
GPIO_ClearPinsOutput(GPIOD, 0x4);
GPIO_SetPinsOutput(GPIOD, 0x8);
DELAY;
GPIO_ClearPinsOutput(GPIOD, 0x8);
}
GPIO_ClearPinsOutput clears all outputs for about 0.5 usec which is not acceptable.
The question is if I missed something in fsl_gpio.h API?
Thanks
Shaul
Hello Shaul,
- Sorry I can't understand your problem clearly, I checked your code ,
set one pin to 1, after delay , then clear it to 0, is this what you want ?
- About "GPIO_ClearPinsOutput clears all outputs for about 0.5 usec ", so , what do you think is right ?
BR
Alice
Hello Alice
Using Xpresso I have tested two alternatives
1. Direct register access (no SDK API)
In this case I have a sequence of GPIOD->PDOR instructions.
Using logic analyzer the resulted waveforms looks O.K there is no "low" gap in transition between the states.
2. Using API (fsl_gpio.h and fsl_gpio.c)
In my solution I am using a sequence of GPIO_SetPinsOutput(), DELAY and GPIO_ClearPinsOutput().
Here using GPIO_ClearPinsOutput() generates a gap of 0.5 usec between transmission from one state to another and in my case is unaceptable.
I my original old project I used KDS3.2 + KSDK 1.3 (with PE).
In that case I used Bits1_PutVal(Bits1_Ptr……) API instructions.
I checked and I didn't fined something equivalent in MCUXpresso SDK API.
And for this reason I'm using direct register access.
The question is if I missed something in a new API when I tried to use GPIO_WritePinOutput() or GPIO_PinWrite() thinking that they are equivalent to Bits1_PutVal( ).
Thanks
Shaul
Hello shaul,
Thanks for your description, I check the code , there is no difference between the two functions,
all configure the two regsiters "PCOR" and "PSOR"
In Processor Expert of KDS:
In SDK:
BR
Alice
Hello Alice
I have slightly different "Bits1_PutVal()" version
Based on my version, I prepared my function equivalent to Bits1_PutVal().
while(1)
{
Bits1_PutVal(Data[k % 8]);
k++;
DELAY
}
/***************************************************************
Functions Code ****************************************************************/
void Bits1_PutVal(uint32_t Val){
RawVal = Val & Bits1_PORT_VALID_VALUE_MASK; /* Mask output value */
// PDI_Val = GPIO_PinRead(GPIOD, 0);
PDI_Val = GPIOD->PDIR;
TogVal = PDI_Val ^ RawVal;
GPIO_PortToggle(GPIOD, TogVal);
}
The concept is working fine, but I have a problem with the "GPIO_PinRead()" function.
Probably the reason is that I don't know how to use it case case that I want to read the whole port and not a single pin.
I bypassed this with "GPIO->PDIR".
Can you please provide a solution how to use "GPIO_PinRead()" instead of GPIO->PDIR
Thanks
Shaul