IDE and SDK for LPC1519

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IDE and SDK for LPC1519

ソリューションへジャンプ
1,458件の閲覧回数
peterkostadinov
Contributor III

Hello,

According to your web site, it is not recommended to use LPCXpresso, but MCUXpresso instead. In order to use MCUXpresso, it is necessary to install proper SDK, but LPC15xx is not available as option in SDK builder. The file "MCUXpresso Supported Devices Table (Dec 2019).xlsx" specifies LPCOpen to be used, but I was unable to find and install this SDK.

Please, advice.

Best Regards,

Peter

ラベル(1)
タグ(1)
0 件の賞賛
1 解決策
1,386件の閲覧回数
ErichStyger
Senior Contributor V

The LPC1519 (and other LPC devices) come pre-installed with the MCUXpresso IDE:

pastedImage_1.png

No SDK needed.

I hope this helps,

Erich

元の投稿で解決策を見る

2 返答(返信)
1,387件の閲覧回数
ErichStyger
Senior Contributor V

The LPC1519 (and other LPC devices) come pre-installed with the MCUXpresso IDE:

pastedImage_1.png

No SDK needed.

I hope this helps,

Erich

1,386件の閲覧回数
peterkostadinov
Contributor III

Thank you very much!

Bets Regards,

Peter

0 件の賞賛