I am trying to build a brushless DC motor controller. It would make my life a lot easier if I could see some demo/example code that does this. Can anyone help me please.
1) MCUXpresso IDE
2) LPCXpresso55S69 Board
3) lpc55S69 uP.
I suspect that the above doesn't exist, is there demo code for other eval boards?
Thanking you in advance.
Hello @philocramer
For BLDC motor control, we highly recommend you using MCXA153. Do not recommend using LPC55s69.
There is application note you can refer to:
https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true
BR
Alice
Thanks for the attempt, but that link is broken. I already have a bunch of application notes & library for BLDC. I was hoping that there exists some eval board that runs a brushless DC motor, so is there any eval board that has demo code for running a BLDC?
I do appreciate your efforts
Philo
Hello @philocramer
Yes, there is FRDM-MCXA153 board.
And there is BLDC motor control application note and code you can refer to.
BR
Alice