Using AppWizard 1.08 with evkb-imxrt1050. We discovered that if an APPW_VAR_OBJECT variable is modified from back-end (UART or SPI) then GUI doesn't receive WM_NOTIFICATION_VALUE_CHANGED until the screen is touched.
Is this is known issue? Is there a workaround (some kind of PostMessage or ForcesUpdate, etc) to trigger the notification?
Attached is a simple example which updates a slider and a text when an ID_VAR_00__IN is modified. ID_VAR_00__IN is incremented when '2' is received from UART, respectively decremented when '1' is received. Can be seen that even the value is modified, the GUI doesn't receive any ID_SCREEN_00__WM_NOTIFICATION_VALUE_CHANGED, unless the screen is touched anywhere. Tried with both libemWin_M7.a (with FP) and libGUI.a (no FP) but same effect.
Please help, thanks!
Daniel
已解决! 转到解答。
Well, we found the bug and it was due what we thought to be an "optimisation". This works:
while (1) {
if (GUI_Exec1()) {
APPW_Exec();
}
APPW_Exec();
}
And this fails:
while (1) {
if (GUI_Exec1()) {
APPW_Exec();
}
}
Seems that the extra APPW_Exec after all GUI_Exec is needed and is the one that helps in getting notifications from variable changing.
Well, we found the bug and it was due what we thought to be an "optimisation". This works:
while (1) {
if (GUI_Exec1()) {
APPW_Exec();
}
APPW_Exec();
}
And this fails:
while (1) {
if (GUI_Exec1()) {
APPW_Exec();
}
}
Seems that the extra APPW_Exec after all GUI_Exec is needed and is the one that helps in getting notifications from variable changing.