I am using the MK22FN512xxx12 (LQFP100) processor connected to an Intel 8080 type LCD interface.
16 bit Data FBD[15..0]
1 bit GPIO for Register / LCD Data control
Rd, Wr, CS,CLK
I am using the Flexbus setup at 16 bit mode and the configurator tool is giving me warnings about the higher Flexbus pins 16,17,18,19,20,25,26,27,28,29,30,31 which I am not needing.
Is this normal?
解決済! 解決策の投稿を見る。
Hi Gary,
MCUXpresso Config Tools is expecting you to configure address bits in FB_AD but in your case using an LCD you don't need them.
Your program should work fine despite the warnings about those pins.
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Gary,
MCUXpresso Config Tools is expecting you to configure address bits in FB_AD but in your case using an LCD you don't need them.
Your program should work fine despite the warnings about those pins.
Have a great day,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------