I installed Pins Tool of desktop version, but I could use this tool, because I had the following error message.
I think that Pins Tool could not access device information file through our company network. Because Pins Tool can access device information file when I use another network.
Therefore I want to download all of device information file using another network before use Pins Tool.
Can I do that?
Please advise to solve this issue as soon as possible.
Best regards,
Takashima
Yes, you can do that.
When you are outside your company network, create a new (File > New) configuration for all the devices you are interested in. At this time, it will reach out and connect to the server downloads the data to your machine. After that, you don't have to have a connection to the server to work with these devices.
I hope this helps,
Erich
Dear Erich
Thank you for your reply.
I'm FAE of NXP Kinetis MCU, then I need to download device information file over 140 devices.
It is difficult to do that.
I talk with our company's IT division about this issue, they need the following information to solve this issue.
- IP address
- Server name and address
- Port number
Could you please let us know that as soon as possible.
Best regards,
Takashima
Hello, here is the info
IP:104.45.233.9
Name:Kex.nxp.com
Port:80
Regards,
Libor
Dear Libor Ukropec,
Thank you for your reply.
Our company's IT division engineer modified some settings of proxy server and firewall, then I can see board and device list.
But I cannot download the processor database. See below error message.
Please advise to solve this issue as soon as possible.
Best regards,
Takashima
Dear Takashima,
hard to say without knowin your network and proxy configuration. Please take a look to the LOG files located here:
c:\Users\<your-user-name>\.nxp\swtools.log + c:\Users\<your-user-name>\.nxp\nxp_conf_workspace\.metadata\.log and post it here so I can look if there's any evident problem or not (if the logs are big, please zip them).
Regards,
Libor
Hello,
Hello Markus,
first few things to verify
1) are you behind a proxy in your work environment? If yes, does it require credentials?
2) from the log I can see you are using Pins tool version 2. Currently supported version is already v4. Is there a specific reason why you stick with older version?
3) "Version 1 files are not supported" I can see just warning message that if you save it with newer tool, it might not work in older tool (tools should be backward compatible, not forward compatible)
Back to the proxy, if you have http proxy which does not require name and password, you can specify it in this file
c:\nxp\i.MX_Pins_v2\bin\tools.ini
fragment of tools.ini (probably the java.net.useSystemProxies should be set to false)
-Djava.net.useSystemProxies=true
-Dhttp.proxyHost=somecompany.proxy.net
-Dhttp.proxyPort=80
More details about specifying the proxy can be found on Oracle web site: Networking Properties
And as a last resort if you provide the board/processor you would like to use I can prepare offline ZIP archive which you can download and manually extract into proper directory.
Regards,
Libor
Hi,
for me this was not working, but it was a good hint.
I added these two additional lines:
-Dhttps.proxyHost=<server address>
-Dhttps.proxyPort=<server port>
hope this helps someone in the future.
regards
Sebastian