MCUXpresso Config Tools v12 Now Available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Config Tools v12 Now Available

2,217 Views
petrstruzka
NXP Employee
NXP Employee

We are pleased to announce that MCUXpresso Config Tools v12 are now available.

Downloads

Revision History

12.0

  • 12.0
    • The product is based on Eclipse 2021-12
    • Enabled EcmaScript 6 script engine
    • Supported Override outpath of files generated by tools
    • Project clonner
      • Added support for SDK 2.12
    • TEE tool
      • i.MX 8ULP applications processor family is now supported:
        • Implemented basic XRDC configuration (MRC, MSC, and PAC)
        • Additionally implemented Process Identifier, TSM, and SP4SM configuration
        • Hybrid templates updated for XRDCs MRC that can be edited by the user and selected by the code region
      • Fixes for the KW45 family:
        • Fixed the bug where LK1 bit in TRDC_CR is not set when all the GVLD bits are set
        • Fixed the bug where setting a lock in Access Templates does not work
        • Fixed the bug where setting ID bypass of a master does not set the bit in its MDA register in the Registers view
      • Fixes for LPC55S and RT5xxS/6xxS families:
        • Fixed the bug where the NSC region is not shown correctly
        • Other minor improvements and fixes
    • Pins tool
      • Added the command to create a function with default routing of pins and signals
      • Created the External User Signals view
      • Added an option to change pins labels in the package view
    • Peripherals tool
      • Fixed the problem with "*/" in the string setting or the instance's comment
      • Components may add instance of another component if required by the component
      • Migration will not change the initialization order
    • Clocks tool
      • Added an option to override locked values to the Import registers dialog
      • Improved behavior of changing global configurations elements in the Functional group properties dialog
    • Minor improvements and fixes
      • Added support for MEX files in comparison to the Update code dialog
  • Overview of Data for Config Tools v12:
    •  
    • General
      • Support of SDK 2.12
      • Support of RT1061xxxB/RT1062xxxxB
    • Pins tool
      • Support of disable states for LPC processors needed to support pins and signals default routing
      • Improved labels of expansion headers
      • Bugfixes and minor improvements
    • Clocks tool
      • Bugfixes and minor improvements
    • Peripherals tool
      • Register init. Components
        • New SEMC register init. component for future integration with memory validation tool
        • Bugfixes and minor improvements
      • SDK init. Components
      • Improved initialization of MPU on Kinetis and i.MX RT processors via new configuration in Global settings
      • Bugfixes and minor improvements
    • TEE tool
      • Bugfixes and minor improvements
    • Memory validation tool
      • Support of Layerscape LX2/LA families

Community

MCUXpresso Config Tools

0 Replies