Config Tool creates generated files in subproject

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Config Tool creates generated files in subproject

856 Views
tsparber
Contributor II

Hello,

we have the following code Structure of a MCUXpresso Project.

Root/board/clock_config.c

Root/board/clock_config.h

Root/board/periperals.c

Root/board/periperals.h

Root/board/pin_mux.c

Root/board/pin_mux.h

Root/source/firmware_main.cpp

Root/Tools/bootloader/project/bootloader/board/

Root/Tools/bootloader/project/bootloader/board/clock_config.c

Root/Tools/bootloader/project/bootloader/board/clock_config.h

Root/Tools/bootloader/project/bootloader/board/periperals.c

Root/Tools/bootloader/project/bootloader/board/periperals.h

Root/Tools/bootloader/project/bootloader/board/pin_mux.c

Root/Tools/bootloader/project/bootloader/board/pin_mux.h

Root/Tools/bootloader/project/bootloader/board/firmware_main.cpp

Root/Tools/bootloader/project/bootloader/bootloader.mex

Root/firmware.mex

In the root folder there is the firmware and in a subfolder Tools there is the bootloader.

Both projects contain a .mex file. Upon code generation the Config Tools always write into the Tools/bootloader subfolder even for the Firmware Project.

Is there a way to configure in which folder the generated code is placed?

pastedImage_1.png

I would expect: Firmware.mex writes to Root/board and bootloader.mex writes to Root/Tools/bootloader/project/bootloader/board/.

The problem started to occur now, as we integrated boot projects into one folder tree.

2 Replies

689 Views
tsparber
Contributor II

I'm able to build just fine, as the bootloader subproject is "excluded from build".

I found a solution / workaround -> Exclude the Subfolder using the Resource Filters

pastedImage_1.png

689 Views
marek-trmac
NXP Employee
NXP Employee

Hi Tommy,

can you build you application?

Currently ConfigTools consider all files inside the project folder as "project files" and returns first clock_config.c that is found.

I'm not aware of any workaround, I'd recommend to split projects into two separate folders.

Regards

Marek

Regards,
Marek
0 Kudos