LPCXpresso54628 No Meil Build *.BIN To Bootloader

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPCXpresso54628 No Meil Build *.BIN To Bootloader

726 Views
spu12kimo
Contributor I

How do I need to burn to LPCXpresso54628 without using Meil build to * .bin through YModem file transfer protocol?
Is it OK to use only MCUXpresso IDE?
Thank 

0 Kudos
1 Reply

626 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hello 寶凱 李, 

I suppose that you are using the AN12384  LPC5460x UART Secondary Bootloader using YModem, which illustrates

how to build your bin file using Keil IDE. To use MCUxpresso you will need to port your source files into a new project and use its tools to generate the bin file.


Have a great day,
Diego

-------------------------------------------------------------------------------

Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos