Incorporating half-duplex (echo suppression) support in blhost

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Incorporating half-duplex (echo suppression) support in blhost

1,252件の閲覧回数
robertpoor
Senior Contributor I

In our application, we need blhost to do firmware updates on a KL27Z via a half-duplex serial line (RS-485, a common industrial standard).  To make blhost work on a half-duplex line, we've extended blhost to "suppress echoes", or more accurately, blhost ignores a received packet if it's identical to the packet just transmitted.  This feature is enabled via a -e/--echosuppress flag on the command line.

So that all works and has proven to be robust.

Our question: since there are certainly other clients working with RS-485 and half-duplex serial lines, is there any interest in back-porting echo suppression into the main branch of blhost?  And if so, what's the procedure for doing so?  

タグ(1)
0 件の賞賛
返信
0 返答(返信)