Will fsl-image-ubuntu be incompatible with s32v234sbc in the future?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Will fsl-image-ubuntu be incompatible with s32v234sbc in the future?

3,725 次查看
seanfung
Contributor II

Dears

What machine is fsl-image-ubuntu currently compatible with? Where can I see a list of compatible machines? Will fsl-image-ubuntu be compatible with s32v234sbc in the future? When will it be supported?

Thanks

Shuo

标签 (1)
0 项奖励
回复
2 回复数

3,609 次查看
Damienl
Contributor I


FSL is available ready to run for Mac OS X and Linux (Centos or Debian/Ubuntu) - with Windows computers being supported via the Windows Subsystem for Linux (WSL). We also provide source code if you run an OS not directly supported by us.

标记 (1)
0 项奖励
回复

3,600 次查看
Damienl
Contributor I

Thanks for this reply bp credit card

标记 (1)
0 项奖励
回复