SBC-S32V234: MIPI connector - current limit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SBC-S32V234: MIPI connector - current limit

跳至解决方案
1,575 次查看
sarawoo
Contributor I

how much current can be provided by the 5V on pin 1 and 3 on the MIPI A connector on the eval board. and how much current can be provided by the 5V/12V pins 25 and 27 on the same connector?  i am using the SBC-S32V234 eval board.  thanks!

标签 (1)
0 项奖励
1 解答
1,423 次查看
KushalShahNXP
NXP Employee
NXP Employee

Hi Sara,

Pins 1 and 3 of MIPI A are connected to 5V supply rail which can drive upto 3A. But it is limited by consumption of the other components connected to 5V and other rails.

Same as above applies to pins 25 and 27. 12V rail can have maximum of 3.3A and is the main supply to other rails. So actual current on these pins are limited by power requirements by other rails.

I hope that helps.

Regards,

Kushal

在原帖中查看解决方案

0 项奖励
1 回复
1,424 次查看
KushalShahNXP
NXP Employee
NXP Employee

Hi Sara,

Pins 1 and 3 of MIPI A are connected to 5V supply rail which can drive upto 3A. But it is limited by consumption of the other components connected to 5V and other rails.

Same as above applies to pins 25 and 27. 12V rail can have maximum of 3.3A and is the main supply to other rails. So actual current on these pins are limited by power requirements by other rails.

I hope that helps.

Regards,

Kushal

0 项奖励