SBC-S32V234: MIPI connector - current limit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SBC-S32V234: MIPI connector - current limit

Jump to solution
1,653 Views
sarawoo
Contributor I

how much current can be provided by the 5V on pin 1 and 3 on the MIPI A connector on the eval board. and how much current can be provided by the 5V/12V pins 25 and 27 on the same connector?  i am using the SBC-S32V234 eval board.  thanks!

Labels (1)
0 Kudos
Reply
1 Solution
1,501 Views
KushalShahNXP
NXP Employee
NXP Employee

Hi Sara,

Pins 1 and 3 of MIPI A are connected to 5V supply rail which can drive upto 3A. But it is limited by consumption of the other components connected to 5V and other rails.

Same as above applies to pins 25 and 27. 12V rail can have maximum of 3.3A and is the main supply to other rails. So actual current on these pins are limited by power requirements by other rails.

I hope that helps.

Regards,

Kushal

View solution in original post

0 Kudos
Reply
1 Reply
1,502 Views
KushalShahNXP
NXP Employee
NXP Employee

Hi Sara,

Pins 1 and 3 of MIPI A are connected to 5V supply rail which can drive upto 3A. But it is limited by consumption of the other components connected to 5V and other rails.

Same as above applies to pins 25 and 27. 12V rail can have maximum of 3.3A and is the main supply to other rails. So actual current on these pins are limited by power requirements by other rails.

I hope that helps.

Regards,

Kushal

0 Kudos
Reply