how much current can be provided by the 5V on pin 1 and 3 on the MIPI A connector on the eval board. and how much current can be provided by the 5V/12V pins 25 and 27 on the same connector? i am using the SBC-S32V234 eval board. thanks!
解決済! 解決策の投稿を見る。
Hi Sara,
Pins 1 and 3 of MIPI A are connected to 5V supply rail which can drive upto 3A. But it is limited by consumption of the other components connected to 5V and other rails.
Same as above applies to pins 25 and 27. 12V rail can have maximum of 3.3A and is the main supply to other rails. So actual current on these pins are limited by power requirements by other rails.
I hope that helps.
Regards,
Kushal
Hi Sara,
Pins 1 and 3 of MIPI A are connected to 5V supply rail which can drive upto 3A. But it is limited by consumption of the other components connected to 5V and other rails.
Same as above applies to pins 25 and 27. 12V rail can have maximum of 3.3A and is the main supply to other rails. So actual current on these pins are limited by power requirements by other rails.
I hope that helps.
Regards,
Kushal