HotFix: Vision Toolbox for S32V234 1.1.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

HotFix: Vision Toolbox for S32V234 1.1.0

3,460 次查看
paulvlase
NXP Employee
NXP Employee

HotFix_1: "No function or variable is defined 'FileName'" error in nxpvt_build()

 

Problem: When trying to run run_face_detection_camera_main.m

 

Root Cause: Coding building error

 

Workaround:  Update the files attached in the following folders 

 {install_dir}\internals\build\private\nxpvt_build.p
标签 (1)
0 项奖励
回复
4 回复数

3,243 次查看
jim_duan
Contributor II

I am using matlab R2018a. This hotfix doesn't work for it.

Thanks,

0 项奖励
回复

3,244 次查看
18502532079
Contributor I

well, the hot-fix seems not working, i encounter the same error When trying to run run_face_detection_camera_main.m

paulvlase

0 项奖励
回复

3,244 次查看
nxf40536
NXP Employee
NXP Employee

Hi 18502532079@163.com‌,

Can you please tell me which version of MATLAB you are using ? 

Thank you,

Vlad Dascau

0 项奖励
回复

3,244 次查看
Daniel_Popa
NXP Employee
NXP Employee

iulianbulancea‌ 

nxf40536

Please have a look!

Thanks!

Daniel

0 项奖励
回复