Datasheet of PTB36241G

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Datasheet of PTB36241G

1,037件の閲覧回数
chaunm
Contributor I

Hello,

I have a question about the datasheet of PTB36241G

I see the Vth(i) has two value: 75mV (min) and 150mV (max). It mean: The design has only one Vthreshold and it between 75mV and 150mV or the design has two Vtheshold, the signal will be detected when it > 150mV, and won't be detected when it < 75mV?

Thanks,

Chau

ラベル(1)
タグ(1)
0 件の賞賛
1 返信

945件の閲覧回数
paulvlase
NXP Employee
NXP Employee

Hi chaunguyen‌,

This community is only for NXP Vision Matlab Toolbox.

We support all technical questions via a ticketing system. Please create a support request for this question at www.nxp.com/support using Support Requests option. This will ensure the correct answer from the subject expert.

0 件の賞賛