RSDK demo for s32r274,Ethernet port is not working.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RSDK demo for s32r274,Ethernet port is not working.

6,349 Views
chenmin1
Contributor II

The program RSDK demo will get stuck when it runs to ENET_DRV_Init(..) - > ENET_Reset(base),

pastedImage_1.png

the value of "base" is obviously wrong.

In "AN5251.PDF", I have found that Ethernet RMII Reference Clock doesn't need to be set on KSZ9031RNX, but it has been set to PG[11]-input and cannot be modified。

pastedImage_3.png

In addition, the green light of the ENET port is off when connected to the Internet cable(I'm testing on S32R274 EVB without motherboard)。

who can help me?

thanks

6 Replies

5,991 Views
Waynel
Contributor I
D
0 Kudos
Reply

4,735 Views
Michael585
Contributor I

I completely like your gave limits as the post you passed on has some extraordinary data which is absolutely basic for me.

0 Kudos
Reply

6,110 Views
mihailcatalinmi
NXP Employee
NXP Employee

Hello,

Please try first the ethernet demo example provided with Platform SDK to see if ethernet is working properly.

Anyway, for RSDK_Demo you need a board with radar frontend(TEF810x), it cannot work on the EVB.

https://www.nxp.com/design/development-boards/automotive-development-platforms/s32r-mcu-platforms/s3... 

Best regards

6,110 Views
chenmin1
Contributor II

Thanks for your answers,I tried enet demo and tcpip demo,also applied tcpip middleware in my project, it work normally.  Only RSDK_Demo will get stuck when writing register,rsdk doc says it can be executed separately without TEF810x. I want to check what is the difference between RSDK and my project。

thanks

0 Kudos
Reply

6,110 Views
chenmin1
Contributor II

pastedImage_1.png

I chang rsdk demo tcpip middleware to the default setting like lwip demo,the green light of the ENET port will be on,bug it also get stuck when runs to ENET_DRV_Init(..) - > ENET_Reset(base)。

0 Kudos
Reply

6,110 Views
Daniel_Popa
NXP Employee
NXP Employee

danielsilion‌,

FYI

0 Kudos
Reply