what is the frequency of IFC module input clk

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

what is the frequency of IFC module input clk

跳至解决方案
966 次查看
shawn_tao
Contributor I

in the codewarrior, why do I set platform clk : sys_clk ratio = 3:1, the platform clk is 200MHz? my physical sys_clk is actual 100MHz, where to change sys_clk input in the code warrior?

pastedImage_1.png

in the manual reference,  does the IFC module input clk equal to the paltform clk?

pastedImage_2.png

in the datasheet, there's a notice in the below, does the IFC module input clk equal to half of the paltform clk?:

pastedImage_3.png

标签 (1)
0 项奖励
回复
1 解答
917 次查看
ufedor
NXP Employee
NXP Employee

SYSCLK.jpg

In the Data Sheet it is written "IFC module input clock (platform clock / 2)" - "/ 2" is a typo.

Correct:

IFC module input clock (platform clock)

在原帖中查看解决方案

0 项奖励
回复
1 回复
918 次查看
ufedor
NXP Employee
NXP Employee

SYSCLK.jpg

In the Data Sheet it is written "IFC module input clock (platform clock / 2)" - "/ 2" is a typo.

Correct:

IFC module input clock (platform clock)

0 项奖励
回复