Hi everyone, I have question about customizing the u-boot in LSDK. I can use flex build to build the deault pack now ,but I have to modify u-boot setting , I review the user guide about LSDK. but there are only operation about linux coustomize,but how to modify the U-boot? I use following step to modify the config for uboot.
1. export ARCH and CROSS-COMPILE enviorment variable
2.cd /packages/firmware/u-boot
3.run make menuconfig to save config
4. run flex-builder -c uboot -m xxxx -b sd
then there is an error at step 4, the error message is
xxxx/flexbuild_lsdk2012/packages/firmware/u-boot is not clean, please run 'make mrproper'
in the 'xxx/flexbuild_lsdk2012/packages/firmware/u-boot' directory.
xxx/flexbuild_lsdk2012/packages/firmware/u-boot/Makefile:1759: recipe for target 'prepare3' failed
make[2]: *** [prepare3] Error 1
who can give me suggestion about it? Thank you!
已解决! 转到解答。
I use LS1046ARDB as an example.
1. $ flex-builder -c uboot -m ls1046ardb -b sd
2. Go to folder packages/firmware/u-boot/, please customize file configs/ls1046ardb_sdcard_defconfig according to your requirement.
3. Rebuild u-boot.
$ rm -rf build/firmware/u-boot/ls1046ardb/
$ flex-builder -c uboot -m ls1046ardb -b sd
Please go to folder "xxxx/flexbuild_lsdk2012/packages/firmware/u-boot" to run "make mrproper" to clean u-boot source code.
No need to run step 3, when execute command "flex-builder -c uboot -m xxxx -b sd", the command "make <target>_sdcard_defconfig" will be invoked automatically.
Dear yiping:
if I use make mrproper to clean it All config will be clear, but I had changed the u-boot config by menuconfig. without the step 3, how can I customize the u-boot conifg? please give me suggestion. Thank you!
I use LS1046ARDB as an example.
1. $ flex-builder -c uboot -m ls1046ardb -b sd
2. Go to folder packages/firmware/u-boot/, please customize file configs/ls1046ardb_sdcard_defconfig according to your requirement.
3. Rebuild u-boot.
$ rm -rf build/firmware/u-boot/ls1046ardb/
$ flex-builder -c uboot -m ls1046ardb -b sd
I follow your instructions:
++ rm -rf build/firmware/u-boot/ls1088ardb/
++ flex-builder -m ls1088ardb_pb -b qspi -c uboot
MACHINE: ls1088ardb_pb
BOOTTYPE: qspi
COMPONENT: uboot
make: Nothing to be done for '/host/opt/LS1088/flexbuild_lsdk2108//packages/firmware'.
make: 'uboot' is up to date.
I also did "bld clean-firmware" but the reswult is the same.
The LSDK is 21.08.
Please, help!