With two place in common, the second macro definition "NXP_DRAM1_ADDR" "NXP_DRAM1_MAX_SIZE ",should be modified as follows
NXP_DRAM1_ADDR--->NXP_DRAM2_ADDR
NXP_DRAM1_MAX_SIZE ->NXP_DRAM2_MAX_SIZE
static void populate_dram_regions_info(void)
{
long long dram_remain_size = dram_regions_info.total_dram_size;
uint8_t reg_id = 0;
dram_regions_info.region[reg_id].addr = NXP_DRAM0_ADDR;
dram_regions_info.region[reg_id].size =
dram_remain_size > NXP_DRAM0_MAX_SIZE ?
NXP_DRAM0_MAX_SIZE : dram_remain_size;
if (dram_regions_info.region[reg_id].size != NXP_DRAM0_SIZE)
NOTICE("Incorrect DRAM0 size is defined in platform_def.h\n");
dram_remain_size -= dram_regions_info.region[reg_id].size;
dram_regions_info.region[reg_id].size -= (NXP_SECURE_DRAM_SIZE
+ NXP_SP_SHRD_DRAM_SIZE);
assert(dram_regions_info.region[reg_id].size > 0);
/* Reducing total dram size by 66MB */
dram_regions_info.total_dram_size -= (NXP_SECURE_DRAM_SIZE
+ NXP_SP_SHRD_DRAM_SIZE);
#if defined(NXP_DRAM1_ADDR) && defined(NXP_DRAM1_MAX_SIZE)
if (dram_remain_size > 0) {
reg_id++;
dram_regions_info.region[reg_id].addr = NXP_DRAM1_ADDR;
dram_regions_info.region[reg_id].size =
dram_remain_size > NXP_DRAM1_MAX_SIZE ?
NXP_DRAM1_MAX_SIZE : dram_remain_size;
dram_remain_size -= dram_regions_info.region[reg_id].size;
}
#endif
#if defined(NXP_DRAM1_ADDR) && defined(NXP_DRAM1_MAX_SIZE) //
if (dram_remain_size > 0) {
reg_id++;
dram_regions_info.region[reg_id].addr = NXP_DRAM1_ADDR;
dram_regions_info.region[reg_id].size =
dram_remain_size > NXP_DRAM1_MAX_SIZE ?
NXP_DRAM1_MAX_SIZE : dram_remain_size;
dram_remain_size -= dram_regions_info.region[reg_id].size;
}
#endif
reg_id++;
dram_regions_info.num_dram_regions = reg_id;
}