support for ls1021aiot in QorIQ SDK v1.9

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

support for ls1021aiot in QorIQ SDK v1.9

1,180 次查看
lucroy
Contributor III

Any plans to support ls1021aiot in the latest release of QorIQ SDK v1.9?

Otherwise is there any patch available?

标签 (1)
1 回复

802 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Luc Roy,

The latest QorIQ SDK release v1.9 doesn't include LS1021AIOT.

Currently you could download LS1021AIoT SDK V1.8 release(for CPU v1.0) and LS1021A-IOT SDK 0.4(for CPU 2.0) from QorIQ LS1021A-IoT Gateway Reference Design|NXP​.

If you require some specific Kernel patches from SDK 1.9 for LS1021, you could use the following method.

Please download SDK 1.9 source ISO, and set up the build environment for LS1021ATWR, run the command "bitbake virtual/kernel -c patch -f" to get the Kernel source in build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux/linux-qoriq/3.12-r0/git, use “git log" command to get the patch list, and use "git format-patch <commit_id>" to get the specific patch.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励