ppa-optee for ls1012afrdm

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ppa-optee for ls1012afrdm

918 Views
mukunkong
Contributor I

Recently,I use layerscape compile ppa-optee for device ls1012a-frdm,while have touble that lsdk1806 only supoort ls1012ardb、ls1012afrwy、ls1043rdb、ls1046rdb,someone who has experience with add new device for optee-os,because i find ppa supportting wtih ls1012afrdm

                                                                                                                                                                                                                                                                                 thanks

0 Kudos
Reply
1 Reply

655 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello 穆 昆空,

FRDM-LS1012A DRAM start address is 0x8000_0000, size is 446M(0x1BE00000).

In the file core/arch/arm/plat-ls/platform_config.h, please add the following definition.

#if defined(PLATFORM_FLAVOR_ls1012afrdm)

#define DRAM0_SIZE                      0x1BE00000
#define CFG_DDR_TEETZ_RESERVED_START    0x97E00000
#define CFG_DDR_TEETZ_RESERVED_SIZE     0x04000000
#define CFG_TEE_RAM_VA_SIZE             (2 * 1024 * 1024)
#define CFG_PUB_RAM_SIZE                (2 * 1024 * 1024)
#define CFG_TEE_CORE_NB_CORE            1
#endif

Please modify the file core/arch/arm/plat-ls/conf.mk to add the following.

ifeq ($(PLATFORM_FLAVOR), ls1012afrdm)
CFG_HW_UNQ_KEY_REQUEST ?=y
include core/arch/arm/cpu/cortex-armv8-0.mk
endif

Thanks,

Yiping

0 Kudos
Reply