The LS1043ARDB board does not have QSPI Flash.
I have tested the LS1046ARDB board. This board contains two QSPI NOR Flashes.
Attached file contains snapshot for the "cat /proc/mtd" command.
This snapshot shows that NXP Linux BSP supports MTD partition.
See also attached .dts file for the LS1046ARDB board.
Have a great day,
Pavel Chubakov
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
I wanted to write and read to qspi using mtd commands from linux space in LS1046ARDB Kit. I tried with mtd_debug command and it was coming as command not found