lsdk1906, ls1028A: No eth0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

lsdk1906, ls1028A: No eth0

750 次查看
ZippZapp
Contributor II

After much struggles getting a functioning sd card image built with lsdk1906 (with firmware from bsp0.3) to boot into ubuntu on a LS1028ARDB, the next problem appears: No eth0!

Felix, ocelot and ENETC drivers are nowhere to be found in lsdk1906.

Can someone please point me in the right direction to fix this?

Thanks!

root@localhost:~# ip a
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default qlen 1000
    link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
    inet 127.0.0.1/8 scope host lo
       valid_lft forever preferred_lft forever
    inet6 ::1/128 scope host
       valid_lft forever preferred_lft forever
2: sit0@NONE: <NOARP> mtu 1480 qdisc noop state DOWN group default qlen 1000
    link/sit 0.0.0.0 brd 0.0.0.0
3: can0: <NOARP,ECHO> mtu 16 qdisc noop state DOWN group default qlen 10
    link/can
4: can1: <NOARP,ECHO> mtu 16 qdisc noop state DOWN group default qlen 10
    link/can
5: docker0: <NO-CARRIER,BROADCAST,MULTICAST,UP> mtu 1500 qdisc noqueue state DOWN group default
    link/ether 02:42:13:22:94:e3 brd ff:ff:ff:ff:ff:ff
    inet 172.17.0.1/16 brd 172.17.255.255 scope global docker0
       valid_lft forever preferred_lft forever

        TX packets 7120  bytes 505544 (505.5 KB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0

root@localhost:/# ethtool eth0
Settings for eth0:
Cannot get device settings: No such device
Cannot get wake-on-lan settings: No such device
Cannot get message level: No such device
Cannot get link status: No such device
No data available

other experiments:

root@localhost:/# modprobe fsl-enetc
modprobe: FATAL: Module fsl-enetc not found in directory /lib/modules/4.19.46

root@localhost:/# ls-addni -n
error: Did not find a device file
Restool wrapper scripts only support the latest major MC version
that currently is MC10.x. Use with caution.
error: Did not find a device file

标签 (1)
标记 (2)
0 项奖励
回复
1 回复

596 次查看
yipingwang
NXP TechSupport
NXP TechSupport

Hello Bjørn Medhus,

Ethernet cannot work with LSDK 1906 on LS1028 platform, this is a known issue.

Please continue to use LS1028 BSP 0.3. LSDK1906 doesn't support LS1028 platform.

Thanks,

Yiping

0 项奖励
回复