Hi,
I would like start u-boot directly of the spi nor flash in ls1043ardb. Is this possible?
(I noticed this question, unfortunately the link doesn't work: https://community.nxp.com/t5/QorIQ/Boot-from-SPI-NOR-flash/m-p/635548)
解決済! 解決策の投稿を見る。
LS1043A supports booting from the QSPI interface - refer to the QorIQ LS1043A Reference Manual, Table 4-9. RCW source encodings.
On the LS1043ARDB there is no SPI Flash connected to QSPI, so booting from SPI Flash is not possible.
LS1043A supports booting from the QSPI interface - refer to the QorIQ LS1043A Reference Manual, Table 4-9. RCW source encodings.
On the LS1043ARDB there is no SPI Flash connected to QSPI, so booting from SPI Flash is not possible.