ls1043ardb: Boot from spi nor flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1043ardb: Boot from spi nor flash

Jump to solution
949 Views
Rasmus
Contributor I

Hi,

I would like start u-boot directly of the spi nor flash in ls1043ardb. Is this possible?

(I noticed this question, unfortunately the link doesn't work: https://community.nxp.com/t5/QorIQ/Boot-from-SPI-NOR-flash/m-p/635548)

0 Kudos
1 Solution
939 Views
ufedor
NXP Employee
NXP Employee

LS1043A supports booting from the QSPI interface - refer to the QorIQ LS1043A Reference Manual, Table 4-9. RCW source encodings.

On the LS1043ARDB there is no SPI Flash connected to QSPI, so booting from SPI Flash is not possible.

View solution in original post

0 Kudos
1 Reply
940 Views
ufedor
NXP Employee
NXP Employee

LS1043A supports booting from the QSPI interface - refer to the QorIQ LS1043A Reference Manual, Table 4-9. RCW source encodings.

On the LS1043ARDB there is no SPI Flash connected to QSPI, so booting from SPI Flash is not possible.

0 Kudos