hi
I can't build ls1021a in yocto,anyone help me ?here is the log;
luhao@ubuntu:/root/LS1021A-SDK-V1.2-20140829-yocto$ source ./fsl-setup-poky -m ls1021atwr -t 4
WARNING: neither of meta-fsl-{ppc,arm} layer locates at /root/LS1021A-SDK-V1.2-20140829-yocto or /root/LS1021A-SDK-V1.2-20140829-yocto/../
ERROR: Specified an invalid machine type!
Usage: . /root/LS1021A-SDK-V1.2-20140829-yocto/fsl-setup-poky <-m machine>
Optional parameters:
* [-j jobs]: number of jobs for make to spawn during the compilation stage.
* [-t tasks]: number of BitBake tasks that can be issued in parallel.
* [-d path]: non-default path of DL_DIR (downloaded source)
* [-c path]: non-default path of SSTATE_DIR (shared state Cache)
* [-b path]: non-default path of project folder (build_${machine}_release)
* [-s string]: append an extra string to project folder
* [-l]: lite mode. To help conserve disk space, deletes the building
directory once the package is built.
* [-p]: append fsl cache and source mirrors (For FSL Internal Use Only)
* [-h]: help
luhao@ubuntu:/root/LS1021A-SDK-V1.2-20140829-yocto$
You seem to be trying to use the SDK as a root. This should not be done. Suggestions:
1. Install and use the SDK as an ordinary user, make sure the installation completes without errors
2. Make sure you executed the host-prepare script before attempting to create a build directory.
3. Do not modify by hand anything in the directory created by the SDK installer.
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi bpe
Thank you very much.I got it with your solution.