how to set LS1043 dpaa's nic card rss hash key (hash key)?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

how to set LS1043 dpaa's nic card rss hash key (hash key)?

890 次查看
Jack2023
Contributor II

We are using LS1043,  our board has ls1043 dpaa nic port,  also have intel i350 port.

there are differences in the rss hash algorithms of network cards from different manufacturers, resulting in the same flow packet not being in the same queue.

Eg: ls1043 is a traffic forwarding device:

client pc <------> eth0 (DPAA nic) <------> eth1 (Intel i350) <------> server pc

for a tcp session,

packet1: client -> server,  the request packet is received to eth0's queue 0,  cpu core 0 process it. (use nxp's rss hash key)

packet2: server -> client,  the response packet is received to eth1's queue 1, cpu core 1 process it. (use intel's rss hash key)

packet 1 and packet2 was processed on different cpu,  will affect performance and other issues.

 

How can I solve this problem by ensuring that the same 5-tuple packet is hashed to the same queue?Can I set the RSS key algorithm for the dpaa nic card  to keep it consistent with i350?

0 项奖励
回复
3 回复数

826 次查看
Jack2023
Contributor II

our application is based on DPDK, there are two solutions:

one solution:

we need a dpaa pmd driver that can customize dpaa nic's rss keys(can modify nic rss key, hash algorithm). we change the dpaa's rss key to same as i350.

Does this solution currently support?

 

second solution:

can you provide the hash algorithm/rss key  for ls1043? so we can modify i350's rss key  to be the same as ls1043's.

0 项奖励
回复

789 次查看
LFGP
NXP TechSupport
NXP TechSupport
You can check the Gianfar driver and adjust it to your needs, please follow the next link to get the driver and its dependences
https://github.com/nxp-qoriq/linux/tree/lf-6.1.y/drivers/net/ethernet/freescale
0 项奖励
回复

855 次查看
LFGP
NXP TechSupport
NXP TechSupport

May be it could be possible, but this is out of scope of initial support, You can try as next:
> one option is to use  ""Ethtool""
The gianfar driver supports the use of ethtool for many configuration options. You must run ethtool only on currently open interfaces. 

> second option
Use  the same driver for both MPU, in our case Gianfar and make the modification on it to fixed to your project.

0 项奖励
回复