Hi All,
I am using LS1043ardb. Right now I am working on the standard board. I am running my application which uses the services ( ssh, snmp and quagga).
I want to know, What are the commands to run these deamons on the board?
By searching I found the below command
/etc/init.d/snmpd/ start
But, I am not getting any init.d folder under /etc
Please help me in getting the proper command to run the above services
Thanks
已解决! 转到解答。
I found the solution myself.
1. quagga is running automatically. No need of any command to start and stop.
2. snmpd can be start and stop using systemctl command
systemctl enable --now snmpd
systemctl disable --now snmpd
3. sshd is running internally
you can check using ssh user_name@ipaddr
but process ID I am not able to check, as in "ps -ef" command I couldnot able to see the sshd running. But scp and ssh command is working
I found the solution myself.
1. quagga is running automatically. No need of any command to start and stop.
2. snmpd can be start and stop using systemctl command
systemctl enable --now snmpd
systemctl disable --now snmpd
3. sshd is running internally
you can check using ssh user_name@ipaddr
but process ID I am not able to check, as in "ps -ef" command I couldnot able to see the sshd running. But scp and ssh command is working
Hi @dibyarekha!
Thank you for contacting NXP Support!
The LS1043ARDB uses Linux and you can learn how to use SSH by following the link:
https://www.ssh.com/academy/ssh/command
Unfortunately, the LS1043ARDB doesn´t have the packages snmp and quagga, you have to compile on Yocto Project to add those packages.
https://www.nxp.com/docs/en/user-guide/LSDKYOCTOUG.pdf
Best Regards!
Chavira