We are looking for ways to reduce power consumption.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

We are looking for ways to reduce power consumption.

Jump to solution
1,023 Views
gyosunshim
Contributor III

Hi,

LS1043A is a system used without FAN, and is looking for a way to reduce power consumption.

I first answered the question by answering the link below.

Is it possible to reduce power consumption by disabling the CPU Core?  

Two additional questions.

First,

Does SWLPM20 mode disable all cores?

Or can I disable individual cores?

I want to run only one core. If you can do that, you would expect a saving of 0.2 x 3 = 0.6 watt.

SWLPM20.png

The second,

Is there a way to do core-specific power gating?

Thank you,

Best regards.

Gyosun.

Labels (1)
1 Solution
960 Views
ufedor
NXP Employee
NXP Employee

> Does SWLPM20 mode disable all cores?

Yes, in SWLPM20 clocks for all cores and platform clocks are disabled.

> Is there a way to do core-specific power gating?

Only PW15.

View solution in original post

3 Replies
960 Views
gyosunshim
Contributor III

Hi ufedor,

Thank you for quick response.

Is there any way to reduce power consumption with software other than lowering PW15 and clock frequency?

Thank you,

Best regards.

Gyosun.

0 Kudos
960 Views
ufedor
NXP Employee
NXP Employee

There are no other methods.

961 Views
ufedor
NXP Employee
NXP Employee

> Does SWLPM20 mode disable all cores?

Yes, in SWLPM20 clocks for all cores and platform clocks are disabled.

> Is there a way to do core-specific power gating?

Only PW15.