VPP show buffers issue on ls1046ardb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

VPP show buffers issue on ls1046ardb

562 Views
skyler
Contributor II

Hey, Guys,

 

I have started VPP on my ls1046ardb board, and did the test cases successfully from lsdk user guide.

Now, I wanna investigate more about performance, so I checked the buffer usage on VPP, but the statistics are very confusing, though the function is all right, packets forwarding right:

vpp# show buffers
Pool Name Index NUMA Size Data Size Total Avail Cached Used
default-numa-0 0 0 2496 2048 16000 15968 34 42949672

vpp# show buffers
Pool Name Index NUMA Size Data Size Total Avail Cached Used
default-numa-0 0 0 2496 2048 8000 8000 0 0

skyler_1-1716375265097.png

skyler_2-1716375347468.png

 

For comparison, I tested the same case on the X86 platform<VPP 21.01>, I can see the "show buffer" works well:

vpp# show buffers
Pool Name Index NUMA Size Data Size Total Avail Cached Used
default-numa-0 0 0 2304 2048 16808 16296 152 360
vpp# show buffers
Pool Name Index NUMA Size Data Size Total Avail Cached Used
default-numa-0 0 0 2304 2048 16808 16296 154 358

 

skyler_0-1716375588141.png

 

So there are two questions:

1, Is the VPP repo in lsdk21.08 the same as https://github.com/nxp-qoriq/vpp/releases/tag/21.08-LSDK and modified from the origin repo https://github.com/FDio/vpp/releases/tag/v21.01 

2. do you guys have any idea about this issue, any relative modifications about buffer pool management you have done?

 

Any replies will be helpful.

Thanks

 

Tags (2)
0 Kudos
Reply
6 Replies

552 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Please refer to NXP latest LSDK release for Layerscape https://www.nxp.com.cn/docs/en/user-guide/LLDPUG_RevL6.1.22_2.0.0.pdf

VPP version is as the following.

VPP v23.02 build with DPDK 22.11.

LLDPUG is based on Yocto, LSDK is based on flex-builder.

LLDPUG is newer than LSDK.

LLDPUG will replace LSDK in feature.

Regards

 

0 Kudos
Reply

517 Views
skyler
Contributor II

hey Bio_TICFSL,

Thanks for the advice, I have booted the latest LSDK release image, and the buffers seem to show right.


But there is another issue, I'm doing the forwarding test by VPP.

Topology:

PC<port0> <-----> <fm1-mac3> ls1046ardb <fm1-mac4> <------> PC<port1>

 

Result:

PC Statistics:

skyler_0-1716809649315.png

 

FM Port:

skyler_1-1716809804406.png

VPP:

skyler_2-1716809847556.png

 

According to the result, you can see the FM port got all the packets, but VPP dpdk-input rx lost  about 1.5M packets, and I can't see anything wrong in vpp.

 

Do you have any idea about where to check the lost packets?

 

Best Regards

Skyler.

 

0 Kudos
Reply

319 Views
Blue_Sky1
Contributor II

Hi,Skyler 

I updated the version of lsdk from lsdk2108 to LLDP RevL6.1.55_2.2.0 ,but it seems that the problem still exists.


  It seems like you updated your version and managed to fix it, I wonder which version you updated?

 

Thanks

0 Kudos
Reply

312 Views
skyler
Contributor II
hey, stupid,

as my hw is ok1046a-c2 from forlinx, there are only forlinx SDK base on lsdk21.08. So I upgrade the dpdk and vpp to 22.11 v23.02 in lsdk 21.08 by manual.
I didn't set up yocto env, so no idea about lldp, sorry for that.

Thanks
0 Kudos
Reply

307 Views
Blue_Sky1
Contributor II
hi,skyler
Thank you very much for your reply!
how did you upgrade the dpdk and vpp to 22.11 and 23.02 on LSDK 21.08?
Thanks
0 Kudos
Reply

501 Views
skyler
Contributor II

Hey, Bio_TICFSL,

 

A few updates:

1) the lost packets is located, all in port_discard_frame </sys/devices/platform/soc/1a00000.fman/1a8a000.port/statistics>

skyler_0-1716864362002.png

 

2) I tested on rgmii port with trex<100% bandwidth>, when frame size is 1518, no frame discard, but once frame size is 64, many discards.

 

As you know, a smaller frame size means more frames. so maybe the frame queue is up to threshold?

 

I'm still working on it.

Any suggestion will be helpful.

 

Best Regards,

Skyler. 

0 Kudos
Reply