Hi,
I use lsdk1812 to compile ls2088a chip, and use buildroot to compile root filesystem, but find the TotalMem is about 5g using "free -g", and our ddr memory is total 8G, so I do not know why is less memory so much, and where is the memory allocation? please give me some advice, thanks very much.
Best Regards
Qiuju.ye
解決済! 解決策の投稿を見る。
The lost DDR can be divided into 2 parts.
1) DDR used by NXP specific software, firmware components
2) DDR used by various segments of kernel.
For the first part,
1) u-boot uses memory till it is used, but once kernel boots, u-boot is swapped out of memory.
2) 66 MB is used by TF-A
3) MC can use anywhere between 512M to 2G (it depends on u-boot comandline argument 'mcmemsize'). The parameter mcmemsize defines amount of system DDR to be used by the Management Complex. If this variable is not defined, the compile-time value 0x70000000 or 1.75GB will be the default. Normally, users do not need to set this variable because the default is acceptable.
TF-A+MC is about 1.8G
kernel reserved=(18620K kernel code, 2476K rwdata, 8844K rodata, 5888K init, 993K bss, 406712K reserved, 327680K cma-reserved) = 771213K=0.7G
The lost DDR can be divided into 2 parts.
1) DDR used by NXP specific software, firmware components
2) DDR used by various segments of kernel.
For the first part,
1) u-boot uses memory till it is used, but once kernel boots, u-boot is swapped out of memory.
2) 66 MB is used by TF-A
3) MC can use anywhere between 512M to 2G (it depends on u-boot comandline argument 'mcmemsize'). The parameter mcmemsize defines amount of system DDR to be used by the Management Complex. If this variable is not defined, the compile-time value 0x70000000 or 1.75GB will be the default. Normally, users do not need to set this variable because the default is acceptable.
TF-A+MC is about 1.8G
kernel reserved=(18620K kernel code, 2476K rwdata, 8844K rodata, 5888K init, 993K bss, 406712K reserved, 327680K cma-reserved) = 771213K=0.7G
Hi yipingwang,
If I modify the mcmemsize to 512M, whether it effects Management Complex to run normally?
Best Regards
Qiuju.ye