My original question is on this forum under a related header, but it seems to have died. Perhaps this is because after someone posts to a question it falls into an "Assumed Answered" state regardless.
----------------------------------------------------------------------------------------------------------------------------------------------------------
Is there not a way to do this without making the change permanent? Writing to the fuses is fine. I just do not want to write to the fuses in such a way as to make it permanent (i.e. making our choice of key permanent).
The manual alludes to a method of doing this by writing to the SRKH shadow registers at boot time (pg 839, section 35.9.3.5). There is an additional step to transfer the mirror register values to the fuse array, but I was under the impression that without doing this final step then the values written to the mirror registers would suffice for secure boot testing.
How we can test secure boot by following the directions on page 8 of this document when we cannot access the SFP registers during secure boot (i.e. per 27.4.2.1 of the LS1043A reference manual)?
In other words, if we intend to boot in a secure way then we must at least configure with SBEN=1 in the RCW. However, according to section 27.4.2.1 we do not actually have read/write access to the SFP registers when booting in secure state. So, it seems that we cannot actually test the chain of trust using the value stored in the SRKH register without permanently writing your key hashes first before attempting a secure boot.
I understand how this would be a huge design flaw in the security architecture of this CPU if it allowed writing to the SRKH registers at boot time while attempting to boot in a secure mode, but it seems reasonable that this should work if the Intent to Secure (ITS) fuse was not set so it all may be tested before making the change permanent.
You can _not_ do this from u-Boot. Secure boot requires a hard reset sequence which returns the mirror registers to their
reset states even if you initialized them before. Booting in core 0 holdoff and initializing registers via JTAG is essential.
The endianness is similar. Now depending if you use uboot (big) or ccs dap/core access (little) or ccs sap access (big). Also, take care abou this: "Write SRKH fuse values into mirror registers. These values must be swapped before writing the
SRKH mirror registers."
This is because SFP_SRKHRn 0-31 >
SRKHR0: key hash bits 255-224
SRKHR1: key hash bits 223-192
SRKHR2: key hash bits 191-160
SRKHR3: key hash bits 159-128
SRKHR4: key hash bits 127-96
SRKHR5: key hash bits 95-64
SRKHR6: key hash bits 63-32
SRKHR7: key hash bits 31-0
Adrian
I think what you have written above might be a mistake. It seems that the first statement "SFP_SRKHRn 0-31" is true and reflects a little endian core. However, the second portion of your port seems to reflect big endianness. Although, I suppose you could also interpret the latter listed format as just informing of which bits align to which register.
So it is clear if anyone come across this and has the same questions, one programs the little endian running LS1043A as:
SRKHR0: key hash bits 244-255
SRKHR1: key hash bits 192-223
SRKHR2: key hash bits 160-191
SRKHR3: key hash bits 128-159
SRKHR4: key hash bits 96-127
SRKHR5: key hash bits 64-95
SRKHR6: key hash bits 32-63
SRKHR7: key hash bits 0-31
From the reference manual it seemed to be quite similar; all the registers referenced in the appnote were identical for the LS1043A. It is really just the SRKH registers that I am concerned with at the moment. I can see from the AN5227 document that the target was big endian. To verify, what is the endianness of the LS1043A? The SDK available has two versions, one having a "-be" extension. That said, the default operation of the LS1043A is then little-endian?
AN5227 appnote that you referred talks about writing to mirror
registers via JTAG and provides steps to do that with CodeWarrior
debugger. As I mentioned in my response to your earlier post,
there is no way to do it in PBL. It is not a security flaw because
JTAG access on production devices can be restricted by by fuses.
Note also that AN5227 is not directly applicable to LS1043A because
it is an ARM v8, not ARM v7 device and requires another CodeWarrior
suite. Details for your chip are currently under NDA, please create a
Support Case to receive additional information:
https://community.nxp.com/docs/DOC-329745
Regards,
Platon
Using a JTAG debugger was exactly how I was planning to do this, just not with the CodeWarrior TAP or development suite for now. I should have provided more information.
Could you provide the specific document for the LS1043A that must be requested under NDA?