正准备使用LS1021,并参考SPF-28673_C1 Demo,有几个问题想请教下:
1、 LS1020的时钟,哪些是必须的,哪些是可选的?
2、 供电芯片MC34VR500V7ES,选择LS1020+DDR4的情况,3.3V供电和Serdes供电会因为电压域原因导致不能同时上电,是否OK?
3、 SPF-28673_C1评估板上在MC34VR500V7ES输出部分使用了2颗INA220AIDGST输出电流/电压/功率监控器,是必须的吗?
4、 SPF-28673_C1评估板上在LS1020A的MAC部分又输入了一路125M时钟,这个是必须的吗?
5、 Serdes有2路时钟,他们与Serdes数据lane对应关系如何?是必须都给的吗?
请帮忙解答下,感谢!
Our customer is using LS1021 and check the reference design of the Demo TWR-LS1021A, SPF-28673_C1
1、 For the clock of LS1020,which must be needed and which one is Optional?
2、 For PMIC MC34VR5100,if as power for LS1020+DDR4, support for both 3.3V and Serdes is ok or not due to the 2different domain power which can not powered at the same time?
3、 In the SPF-28673_C1, 2pcs INA220AIDGST used as monitor of Voltage and Current at output of MC34VR500V7ES,so INA220 must be needed?
4、 In the SPF-28673_C1, another 125M clock is used for MAC of LS1021A, tt's necessary?
5、 For the 2clock for Serders ,how about the relationship about the Serdes' LANS? It's necessary?
1) Please refer to the QorIQ LS1021A Reference Manual, 4.4.7 Clocking to select a clocking mode.
2) The question is not clear.
3) Usage of INA220 is not a must.
4) External 125 MHz reference clock (ECn_GTX_CLK125) is needed if RGMII interface is used.
5) Please refer to the QorIQ LS1021A Reference Manual, Table 33-2. Supported SerDes options, column "Per lane PLL mapping":
"1" corresponds to the PLL1
"2" corresponds to the PLL2
Example:
SRDS_PRTCL_S1 = 0x10
Per lane PLL mapping: 1211
Lanes A, C, D - PLL1
Lane B - PLL2
If PLLn is not used then it has to be powered down and corresponding reference clock is not needed.