We are working on a board using Rev 2.0 of the LS1021A but seem to be running into a problem with QSPI booting.
As per reference manual F, the LS1 will search for the RCW at byte offset 0 of NOR.
We have used a programmer to write, and successfully read back, the PBL (preamble, RCW, and PBI's) to byte offset 0 of NOR.
However, the LS1 continually reads 8 bytes (probed and confirmed that they are the first 8 bytes which we programmed) before resetting itself.
Thank you in advance!
解決済! 解決策の投稿を見る。
Hi Tyler,
PBL obviously does not sample the preamble of RCW correctly.
Check the endianess of your data in QSPI. Endian boundary is 64 bits. Also, rev1 of silicon had issue with timing on QSPI while in PBL. I don't know is this issue still persists in rev2 silicon (it should not), but you can try adding 22p cap to QSPI_DIO_A0 to fix that.
Regards,
Borut
Hi Tyler
I assume this is your custom board. Can you
post your RCW_SRC bootstrap pin settings and
the RCW that you programmed into your SPI NOR ?
Regards
Sinan Akman
Hello Sinan.
You are correct, this is a custom board.
CFG_RCW_SRC0 = 0
CFG_RCW_SRC1 = 0
CFG_RCW_SRC2 = 1
CFG_RCW_SRC3 = 0
CFG_RCW_SRC4 = 0
CFG_RCW_SRC5 = 0
CFG_RCW_SRC6 = 1
CFG_RCW_SRC7 = 0
CFG_RCW_SRC8 = 0
This follows the documentation's required format for QSPI of 0_0100_010X.
The first 72 Bytes in SPI NOR are:
AA55AA55 01EE0100 08080010 00000000 00000000 10000000 10000000 08007922 40025A00 81046000 00000000 00000000 00000000 2003E800 00004504 24BB3140 00000000 00000000
But after reading the first 8 bytes, the LS1 goes into reset.
Hi Tyler,
PBL obviously does not sample the preamble of RCW correctly.
Check the endianess of your data in QSPI. Endian boundary is 64 bits. Also, rev1 of silicon had issue with timing on QSPI while in PBL. I don't know is this issue still persists in rev2 silicon (it should not), but you can try adding 22p cap to QSPI_DIO_A0 to fix that.
Regards,
Borut
This turned out to be the issue.
Performing a 64-bit byte swap to the PBL such that "AA55AA55 01EE0100" became "0001EE01 55AA55AA" allowed the rest of the PBL to be read.
At this point, we have inserted our custom RCW into ls102xa_rcw_sd.cfg in Linux SDK for LS1021A v0.4, taken the PBL from the resulting u-boot-ls1021atwr-2014.07-r0.bin, performed a 64-bit byte swap, and programmed this to SPI NOR. As to be expected, booting fails when the Secondary Program Loader tries to read U-Boot from the SD card.
While possible and partially complete, this process seems a little roundabout. Is there a way to use the SDK to build a PBL for SPI NOR? (setting UBOOT_CONFIG ??= "qspi" in ls1021atwr.conf does not do so)
Hi Tyler
Good to hear you found the problem.
I am just curious, when you say
"We have used a programmer to write ..."
what programmer did you use. I'd expect
the programmer would have done a "swap"
based on the a choice of endianess. Was
there an option for this ?
Regards
Sinan Akman
We are using an Asix Forte Programmer. No endianess swap is performed and there is no option for it. While needing to manually swap bytes isn't convenient, it's certainly not the most important of our concerns.
At the moment, the only PBL we can build using the SDK is one for booting from SD. Is anyone aware of a way to build a PBL for booting from SPI NOR?
Hi Tyler
Thanks for the follow up. At this point
the mainline u-boot (which I primarily
use) does not generate RCWs for NOR
(as well as SPI NOR). In the case of NOR
it expects that RCWs that are shipped with
the board or generated by SDK will be used.
I will send a patch in the coming days to mainline
u-boot to generate an rcw.bin file that is
known to work for NOR boot and I'll see
if I can extend this to SPI NOR with the
right endianess as well.
Regards
Sinan Akman
Hi Sinan
Im also working in ls1021a-IOT board(REV 1). I know that it wont support QSPI booting on REV1. So I'm ordered REV 2 board. In that I need to boot up from QSPI. So can you pls send me the patches to generate the RCW.bin for QSPI(Where the RCW.bin is not generating for QSPI after bitbaking, but it is generating for SD card).
Thanks In advance.......!
In addition, can you please verify that GROUP B PIN
CONFIGURATION (BITS 384-415) of RCW reflects the
SPI pin connections in your design ?
Regards
Sinan Akman
Yes, the Group B Pin Configuration is set appropriately.
Tyler, when you mention "the LS1 continually reads 8 bytes",
do you mean the preamble and the sysaddr or does it actually
read the first 8 bytes of RCW (i.e. 08080010 00000000) ?
Regards
Sinan Akman
Just the preamble and sysaddr.
After reading "AA55AA55 01EE0100", it resets and repeats reading the same 8 bytes.