Hi,
I am trying to test the Seamless redundancy feature in LS1028A RDB, and while running the commands as per the BSPv0.3 document. I always get error saying
tsntool>cbstreamidset --device swp0 --streamhandle 1 --nulldmac 0x7665d268f7d9 --nullvid 1
Type do not supported!
error streamid type: only null stream identify supported now
Complete log is attached below.
The issue will be investigated as Technical Case #00213086
I was able to go past this error by adding an additional parameter
--nullstreamid
with the command, but still the test case doesn't work.
Is there anything else missing in document for this test case?