SERIAL MANAGEMENT BUS OF PCIE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SERIAL MANAGEMENT BUS OF PCIE

606件の閲覧回数
Ellu24
Contributor III

I am designing a hardware using LS1046. While I designing PCIe, I found SMB data and clock of PCIe is connected to host through I2C protocol. Is it necessary to use this SMB in PCIe designing or can I left it unconnected?

 

Thanks in Advance

0 件の賞賛
1 返信

571件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
For detailed information, kindly refer to the "PCI Express Mini Card Electromechanical Specification, Rev 1.2" System Management Bus (SMBus) is optional as per PCIe base specification. The pins assigned to these functions are to be left disconnected if the functions are not implemented.
0 件の賞賛